Good Morning,
I am interested in using the GC5337 for a development project and am unclear if there is (or will be) an SEK similar to the GC5325SEK for the GC5337.
Thanks for your attention,
Ken
Hello,
The GC5337 (GC5330), and GC6016 (GC533x without DPD), have an older combined EVM (meaning integrated data converters and digital on one board), http://www.ti.com/tool/gc6016evm, and there is a newer digital EVM in development.
The GC533x, GC6016 family have DUC functions, so the interfaces are not the same as the GC5325 SEK.
Depending on configuration, repeaters (initial use for GC6016) EVM does not require a TSW3100 Tx input baseband card. The same EVM with a different configuration,
and GC533x device, and a TSW3100 Tx input baseband card, can support Tx BB to RF demonstrations, similar to the GC5325SEK.
Please contact your local TI Field Application Engineer or Distributor to see if the older EVM is available. The newer EVM is not yet released, it may be available late this year.
Regards,
Radio Joe