• Resolved

TSW4100

Guru 11375 points

Hello,

need matlab script that simulates the response of the GC5016 in split IQ & 4 Channels modes.

B.regards

Eli

  • Hello,

    The GC5016 can be operated in DDC or DUC modes.  There are several different modes of operation, within one device, or as on the TSW4100 there are 2 devices,

    one DDC and one DUC.  The DDC&DUC Fundamentals application note, online GC5016 training, Guide for Using cmd5016, and the GC5016 datasheet can be used

    to determine the operating modes.  There is a PFIR and CIC for the filtering and decimation/interpolation. 

    Related to the TSW4100, the decimation ratio and interpolation ratio are common across the repeater channel.  The repeater can be operated in 4 channel mode, or splitIQ 2 channel modes.  SplitIQ means that I and Q are processed in separate DDC/DUC channels.  This increases the number of PFIR taps available.   

    There is no direct Matlab model for the GC5016, there is a set of functional models that provide for

        Cascade Integrator Comb decimation and interpolation

        PFIR decimation and interpolation

    The cmd5016 program will need to be run with the desired splitIQ, cic_dec, cic_int, pfir_dec, pfir_int ratios to determine the allowed number of PFIR taps.

    DDC

        Complex Mixer

        CIC dec

        PFIR dec

        BB Gain (bbAGC is not supported in model equivalent)

    DUC

        BBGain

        PFIR interp

        CIC interp

        Complex Mixer

        Channel summer (1 to 4 channels, and scaling) - not supported in model equivalent

    The attached script creats a convolved response of the PFIR filter, CIC and allows the user to observe the spectral response of the filter.   The CIC response is estimated in the matlab script.   In the matlab script, there are 2 DDC examples, and 2 DUC examples, 1 DDC 4chan, 2 DDC splitIQ, 3DUC 4chan, 4DUC splitIQ

    The GC5016 datasheet has the calculation of the number of clocks, the cmd5016 tool also has a calculation for the number of taps.  Once you input the cic_dec, cic_int

    pfir_dec, pfir_int, the clock rate, Fs (filter stop half bandwidth), Fp (filter pass half bandwidth), the script can compute the convolved response of the GC5016 filter, and generate the PFIR taps to be used with cmd5016 to program the GC5016.

    Note: the Matlab script requires the Signal Processing Toolbox to generate the filter taps.

    Regards,

     

    Radio Joe

     

     

     

    gc5016_filterdesign_0711.m