Hi,
I got a Problem with the CC1200. The Pins GPIO2 (CCIO_2) and GPIO1 (MISO) (used as part of SPI 2) has a permanent "High" status. I have checked the Pins of connections with the supply voltage or other unintended connections, but all right. Can anyone explaine that?
I hope the chip is not distroyed, it would be difficult to change him.
Greatings Alex
Supplement:
I have detected, that between the supply layer and the pins are only a resistence of 4.2 ohm. It looks like an electrical short. And please I need your aid realy