I know that SOP2 has to be pulled high to program the CC3200MOD's internal flash, and that the state of SOP[2:0] is specified nominally as 100 for programming, but I can't find any specific confirmation that SOP0 must be low (in addition to SOP2 being high) for programming. This would mean that on a board intended to always use 2-wire JTAG and/or SWD, I'll have to be able to not only pull SOP2 high for programming but also pull SOP0 low. If SOP0 is actually "don't care" when SOP2 is high then that would simplify things.
Thanks,
Julia