Hello,
I'm using a SmartRF04EB 1.9 board with the CC1101 RF board. I am attempting to connect to this via my host (Ubuntu) machine and share the connection with a virtualized windows 7 box to run SmartRF Studio. The board is powered on and I receive a status on the LCD display however there is no entry for it in /dev so I am unable to share it. Are there any basic linux drivers that can be used to set this up? Or am I strictly required to use a Windows host machine.