PAN1325 SLOW_CLK_IN

The SLOW_CLK_IN on the PAN1325 module is labeled as Fail Safe.  Does this mean that I do NOT hve to provide a clock?  That would be the implication ....

 

Also, would the LDO 1.8V output supply enough current to run the VDD_IO?  I see no real information regarding this option.  I have been relying on the PAN1315 app sheet which seems a bit more complete but am not sure if I should trust it.  Is there a more complete data sheet for the PAN1325 that gives full AC/DC specs and more information of OPTIONS, etc.?

 

Thanks for your help,

 

Mark