This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm working on a front-end for an SDR radio receiver. Most ADCs have input ranges in the order of volts, while the antenna signal can be as low as a fraction of a uV. I wonder if it's the way to go to amplify these signals by 120 dB (!?) without creating other problems in the circuit. Or is it that only voltage is amplified by not power (or not that much)?
Regards
I found in an app note, they use an 1:4 transformer with a -3 dBm input @ 50 ohm to feed the ADC differential input with 2V4 reference.