Hello all,
In my project, i will build a zigbee sensor network size of 100+. I am planning to read data from sensors using msp430 and share the sensor data in zigbee network. As a starting point, i am planning to build a small zigbee network using cc2530 mini znp kits. And i am making plans of using msp 430 in that kit to read sensors and share the data in zigbee network built with cc2530 in the kits. Is it a rational starting point? And also i have no idea what is the maximum size of network that is built with cc2530 tranceivers?could you share your precious opinions with me??