Hello,
when i left my desk on friday evening, everything was fine. But since i started this morning, i am not able to get a connection using BTool and the USB-Dongle (HostTestApp).
I have installed a Serial-Logger to capture the communication between BTool and the Dongle. This didn't work and I've already uninstalled the utility. I'm not sure if this "damaged" somehting? I didn't change anything else since friday. I tried to reinstall the CDC-Driver, reflashing the Dongle, system reboot etc. but nothing seems to help.
UPDATE: I also tried to use my own PCB (equal to the Dongle's reference design) with HostTestApp and i got the same problem as with the original dongle. So the hardware isn't the problem. As i wrote before, i uninstalled the serial logger but it didn't help.
Thank you very much!
Port opened at 16.01.2012 14:02:44[1] : <Tx> - 02:02:45.157-Type : 0x01 (Command)-Opcode : 0xFE00 (GAP_DeviceInit)-Data Length : 0x26 (38) byte(s) ProfileRole : 0x08 (Central) MaxScanRsps : 0x05 (5) IRK : 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00 CSRK : 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00 SignCounter : 0x00000001 (1)Dump(Tx):01 00 FE 26 08 05 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 01 00 00 00 ------------------------------------------------------------------------------------------------------------------------[2] : <Rx> - 02:02:45.303-Type : 0x04 (Event)-EventCode : 0x0E (HCI_CommandCompleteEvent)-Data Length : 0x04 (4) bytes(s) Packets : 0x01 (1) Opcode : 0x0101 (Unknown Op Code) Raw : 01 01 01 01 Dump(Rx):04 0E 04 01 01 01 01 ------------------------------------------------------------------------------------------------------------------------[3] : <Rx> - 02:02:45.348-Type : 0x04 (Event)-EventCode : 0x0E (HCI_CommandCompleteEvent)-Data Length : 0x04 (4) bytes(s) Packets : 0x01 (1) Opcode : 0x0100 (Unknown Op Code) Raw : 01 00 01 01 Dump(Rx):04 0E 04 01 00 01 01 ------------------------------------------------------------------------------------------------------------------------[4] : <Rx> - 02:02:45.392-Type : 0x04 (Event)-EventCode : 0x0E (HCI_CommandCompleteEvent)-Data Length : 0x04 (4) bytes(s) Packets : 0x01 (1) Opcode : 0x0101 (Unknown Op Code) Raw : 01 01 01 01 Dump(Rx):04 0E 04 01 01 01 01 ------------------------------------------------------------------------------------------------------------------------[5] : <Rx> - 02:02:45.446-Type : 0x04 (Event)-EventCode : 0x0E (HCI_CommandCompleteEvent)-Data Length : 0x04 (4) bytes(s) Packets : 0x01 (1) Opcode : 0x0101 (Unknown Op Code) Raw : 01 01 01 01 Dump(Rx):04 0E 04 01 01 01 01 ------------------------------------------------------------------------------------------------------------------------[6] : <Rx> - 02:02:45.497-Type : 0x04 (Event)-EventCode : 0x0E (HCI_CommandCompleteEvent)-Data Length : 0x04 (4) bytes(s) Packets : 0x01 (1) Opcode : 0x0101 (Unknown Op Code) Raw : 01 01 01 01 Dump(Rx):04 0E 04 01 01 01 01 ------------------------------------------------------------------------------------------------------------------------[7] : <Warning> - 02:02:55.045GAP Device Initialization Timeout.Device May Not Function Properly.