Hello 

I am working with CC1101.I have configured my CC1101 in RX mode and it is possible to receive packets sent from CC1101 demo board with 2FSK modulation.But when I use manchester encoding with FSK modulation I am not able to receive any packets.And if I put the same configuration in CC1101 demo board it possible to receive packets with manchester encoding.

My configuration is as follows

#define CC1101_IOCFG2_value	0x06 // assert - sync word transmitted/received, deassert - end of packet
#define CC1101_IOCFG1_value 0x2E // tri-state
#define CC1101_IOCFG0_value 0x01 // assert - RX FIFO is filled at or above the threshold or at End of packet, deassert when TX FIFO is below the threshold
#define CC1101_FIFOTHR_value 0x65F2 // SmartRF Studio
#define CC1101_SYNC1_value 0xD3 //
#define CC1101_SYNC0_value 0x91 // 32 bit SYNC Word value
#define CC1101_PKTLEN_value 0x06 // Indicates Packet Length value
#define CC1101_PKTCTRL1_value 0x00 // SYNC word always accepted,dont Append RSSI and LQI values, no address check
#define CC1101_PKTCTRL0_value 0x00 // Fixed packet length mode without CRC;Data whitening off,Normal mode use of FIFO for RX & TX
#define CC1101_ADDR_value 0x00 // address-00
#define CC1101_CHANNR_value 0x00 // channel no.0
#define CC1101_FSCTRL1_value 0x06 // from smartrf studio
#define CC1101_FSCTRL0_value 0x00 // from smartrf studio
#define CC1101_FREQ2_value 0x21 // Carrier-868.3MHz
#define CC1101_FREQ1_value 0x65 // Carrier-868.3MHz
#define CC1101_FREQ0_value 0x6A // Carrier-868.3MHz
#define CC1101_MDMCFG4_value 0x89 // RX Filter BW- 203 kHz,data rate 17 KBaud
#define CC1101_MDMCFG3_value 0x57 // Data rate-17 KBaud
#define CC1101_MDMCFG2_value 0x0B // 2FSK modulation,32/30 sync word bits, Manchester enable
#define CC1101_MDMCFG1_value 0x22 // Disable FEC, Preamble bytes-4
#define CC1101_MDMCFG0_value 0xF8 // Channel spacing-200 KHz
#define CC1101_DEVIATN_value 0x50 // deviation 50 kHz
#define CC1101_MCSM2_value 0x07 // Timeout for sync word search in RX for both WOR mode and normal RX is until end of packet
#define CC1101_MCSM1_value 0x3F // Next state after finishing packet reception is RX,Clear channel indication if RSSI below threshold unless currently
//receiving a packet
#define CC1101_MCSM0_value 0x18 // Automatically calibrate When going from IDLE to RX or TX