Hi,
I'm running on a custom cc2540 board with no peripherals and external 32khz + 32Mhz crystals.I tried both the SimpleBLEBroadcaster and SimpleBLEPeripheral examples from the BLE 1.3.2 SDK. With both examples, advertisement is 100 ms continuous and works fine when power saving is disabled.
When recompiled with POWER_SAVING though, the board advertises 4 times (100 ms apart), and then the code gets stuck in a loop. The board draws about 9 mA when this happens, and the CPU is stuck in a tight loop somewhere around llStopTimer2 (no source). .
I've seen post about this happening when using the internal RC oscillator, but this isn't the case. Any ideas on what might be happening?