Hi all,
this is the design #5 in the antenna DK.
This is what I measure when I connect this design #5 to my VNA.
I have designed a 868 MHz antenna and I think it may fit my needs but I suspect it could work better. However, it consists of a single-sided trace instead of a double-sided trace as the design #5, where the two traces are put together with vias. This is the performance of my antenna.
So my questions are simple:
- When would be recommended to use double-side as the TI design? Should I do it? I do not think so but what is your opinion? Is the purpose of double-side to have more antenna volume so more efficiency?
- What is your opinion about my measurements? Aren't these too spiky? Would you expect different values for the TI design? Should I re-calibrate?
Have a very nice day! And do not laugh too much, these are my first days with antenna designs :)