Hello,
i am trying to receive following data on the cc1101 in async mode:
I had not any infomation of the transmitter, so i did some analysis:
This looks to me like 2-FSK with 433.92 Mhz an approx. 40Khz deviation.
With the following configuraition i do not receive the upper data:
0x0D, // 00 IOCFG2 0x2E, // 01 IOCFG1 0x2D, // 02 IOCFG0 0x07, // 03 FIFOTHR 0xD3, // 04 SYNC1 0x91, // 05 SYNC0 0x3D, // 06 PKTLEN 0x04, // 07 PKTCTRL1 0x32, // 08 PKTCTRL0 0x00, // 09 ADDR 0x00, // 0A CHANNR 0x06, // 0B FSCTRL1 0x00, // 0C FSCTRL0 0x10, // 0D FREQ2 0xB0, // 0E FREQ1 0x71, // 0F FREQ0 0xC7, // 10 MDMCFG4 0x8B, // 11 MDMCFG3 0x03, // 12 MDMCFG2 0x22, // 13 MDMCFG1 0xF8, // 14 MDMCFG0 0x47, // 15 DEVIATN 0x07, // 16 MCSM2 0x00, // 17 MCSM1 0x18, // 18 MCSM0 0x14, // 19 FOCCFG 0x6C, // 1A BSCFG 0x07, // 1B AGCCTRL2 0x00, // 1C AGCCTRL1 0x90, // 1D AGCCTRL0 0x87, // 1E WOREVT1 0x6B, // 1F WOREVT0 0xF8, // 20 WORCTRL 0x56, // 21 FREND1 0x11, // 22 FREND0 0xE9, // 23 FSCAL3 0x2A, // 24 FSCAL2 0x00, // 25 FSCAL1 0x1F, // 26 FSCAL0 0x41, // 27 RCCTRL1 0x00, // 28 RCCTRL0
Regadrs