given on the TI website,
http://www.ti.com/product/CC1020/technicaldocuments#doctype5
--
Trivesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Trivesh
Looking into the network from the RF_OUT pin with a 50 ohm port for the antenna, I am seeing 19+j13 for 868 MHz. instead of 15+j24. Which one is correct, If i want to design my own matching network what RF_OUT impedance should i consider.
Did you use the PCB with correct stack-up and the model for the correct Murata components when you did this sim? Note that both the PCB and real vs ideal components have an impact on the result.
By using correct murata components in the simulation, I am getting 14+j13.5 instead of 14+j24. This is close but not sufficient to be considered matched.
I have incorporated the receiver circuit as well, and input impedance of receiver circuit from RF_in pin is 50+j1. Here too, RF_in impedance given data is different (54+j23).
please verify this to me.
Thanks
In ADS, import the gerber file for the component layer. Adjust the stack-up to reflect the CC1020 EM.
For exactly how to do this you have to check the ADS documentation.