Hi guys,
I am familiar with the CC430. I used it on a DASH7 platform (433MHz) but was only able to get 100 meter distance. I would like to increase that to the guaranteed 1 Km or more. What chip set is recommended for maximum distance.
Also I read where Europe was able to use 20dB more power in this range. That's a factor of 10 which would increase my distance to 1 Km. Is this true? Am I limited in distance due to american regulation?
Mike