Hello All,
I was considering a miniature PCB antenna -- I found the (http://www.ti.com/lit/an/swra416/swra416.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello All,
I was considering a miniature PCB antenna -- I found the (http://www.ti.com/lit/an/swra416/swra416.pdf
the design note shows gain as 2.33dBi, with measurement @ 868MHz occurring with 0dBm power out, following the EIRP formula and assuming no loss in the circuit because it is directly connected, the value of 2.33dBm is given for EIRP (when operating at 0dBm out, at 868MHz). (reason i bring this up is that i don't see a max indicated here, i just see characterization measurement being presented for reference. You want to know the maximum output power this antenna will support and i think the question is also perhaps better phrased as to include the frequency band you will operate in with regards to its performance, so you get data that is meaningful to you - agree?
Thanks Josh, I agree and the question was not fully phrased. The frequency of interest is at 868MHz.
-Akshay