Hi,
Im intending to read a TRPGR30TGC transponder and I have a board RI-ACC-ADR2-10 using tms3705 . Do you have any source code available for that ?
regards,
Bruno
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
in the LF.c file of the source code given on the web, you just need to comment out the PWM and BLC times used for TMS37157 and add these lines of code
PWMtimes.usToffH = 1000; //timings for RO_RW
PWMtimes.usTonH = 1000;
PWMtimes.usToffL = 300;
PWMtimes.usTonL = 1700;
BLCtimes.usToff = 170;
BLCtimes.usTonL = 230;
BLCtimes.usTonH = 350;
BLCtimes.usTonSC = 600;
then you can hook up a scope and make sure its working correctly according to the attached notes i took