I have an RF circuit built on top of the meandering monopole reference design (#6) in swrr070. However, based on product design concerns, I need to reduce the size of the PCB. I see a few ways of doing so:
- There is a 1.5 cm feedline to the antenna tuning circuit. I understand that this feedline is sized in such a way that it is close to 50 ohms (at least using the calculator at emclab.mst.edu/.../index.html) but I don't understand why the feedline is so long or if it even needs to exist in this circuit. For one, the impedance of the feedline is independent of the length of the feedline. In addition, I don't see why I'm not able to connect the SMA connector directly to the antenna matching circuit/antenna.
- I could possibly use the ceramic antennae which are significantly smaller in size. However, in #3, there is an additional narrower feedline from the antenna matching circuit to the ceramic antenna. Again, is this feedline avoidable? If so, why does it exist in the first place? Is it for better comparisons with the other antenna reference designs?
PS: Took some E&M back in college but I haven't used it in a while. Also, it seems like unlike software/firmware, RF related problems are hard to Google for....