Hi,
ISO/IEC 15693 stipulates read ranges upto 1-1.5m. What is the antenna size I should use with TRF7962A for achieving this read range?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
ISO/IEC 15693 stipulates read ranges upto 1-1.5m. What is the antenna size I should use with TRF7962A for achieving this read range?
EMC regulations and physics of magnetic fields at the operating frequency govern the range - the ISO standard makes no comment on distance.
to get the distance, an antenna in the neighborhood of something larger than 800mm x 600mm could be used with large rectangle tag like our RI-I02-112 product
but, the 200mW max that the TRF79xxA devices put out is not enough power to drive that distance. an amplifier would be needed, and in the range of 4-8W output
power with a suitable receiver for this kind of power out. Good example of a readers and antennas like this comes from Feig Electronics.
Hi,
Many manufacturers are claiming upto 1.5m read range for their ISO 15693 tags. Some examples are as follows:
http://www.st.com/web/en/home/catalog/mmc/FM76/CL1766/SC1204
http://www.adafruit.com/datasheets/rfid%20guide.pdf
In the above links read distance of various types of RFID tags is compared. Is that read distance with the same reader antenna?
Also, if the reader antenna size is too big in the order 800mm x 600mm, then won't it be able to read any HF tag other than ISO 15693? Then what is the point in quoting higher read distances for some tags?