This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650: problem with Zstack library

Other Parts Discussed in Thread: Z-STACK

Hello CC Team,

I'm working with the Zstack library (Home ver 1.2.2) and with the EVB "SamrtRF06 + cc2650EM-7ID rev 1.2".
I've followed the "Z-Stack Home Automation Sample Application User’s Guide" and I've properly compiled the example SampleSwitch.

I have this problem: when I try to erase the memory by going to the menu Project->Download->Erase Memory or when I try to download the code by going to the menu Project->Download>Download Active Application I have always the same error: "Failed to halt after bootloader 2" and "Failed to load flash loader ...FlashCC26xxF128RAM20".

Did I forget some compiler options? Is my hardware revision compatible whit the Zstack library?

Best Regards,
Luca