This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TRF372017: Recommended constant of PLL loop filter for Japanese Terrestrial Digital TV

Part Number: TRF372017

Hi all,
My customer plans to use TRF372017 for Japanese Digital TV.
Could you tell me the recommended constant of PLL loop filter for this application?
Also I would like to know the recommended value of RDIV of TRF372017.

When using the Loop filter calculation tool, should we calculate a constant based on the CH33 of the center channel for this application? 

Reference input frequency: 65.0158MHz

RF Output frequency:

6MHz/ch

CHCarrier frequency (MHz)Occupied band (MHz)
13 473.142857 470.357857 - 475.927857
14 479.142857 476.357857 - 481.927857
15 485.142857 482.357857 - 487.927857
16 491.142857 488.357857 - 493.927857
17 497.142857 494.357857 - 499.927857
18 503.142857 500.357857 - 505.927857
19 509.142857 506.357857 - 511.927857
20 515.142857 512.357857 - 517.927857
21 521.142857 518.357857 - 523.927857
22 527.142857 524.357857 - 529.927857
23 533.142857 530.357857 - 535.927857
24 539.142857 536.357857 - 541.927857
25 545.142857 542.357857 - 547.927857
26 551.142857 548.357857 - 553.927857
27 557.142857 554.357857 - 559.927857
28 563.142857 560.357857 - 565.927857
29 569.142857 566.357857 - 571.927857
30 575.142857 572.357857 - 577.927857
31 581.142857 578.357857 - 581.927857
32 587.142857 584.357857 - 589.927857
33 593.142857 590.357857 - 595.927857
34 599.142857 596.357857 - 601.927857
35 605.142857 602.357857 - 607.927857
36 611.142857 608.357857 - 613.927857
37 617.142857 614.357857 - 619.927857
38 623.142857 620.357857 - 625.927857
39 629.142857 626.357857 - 631.927857
40 635.142857 632.357857 - 637.927857
41 641.142857 638.357857 - 643.927857
42 647.142857 644.357857 - 649.927857
43 653.142857 650.357857 - 655.927857
44 659.142857 656.357857 - 661.927857
45 665.142857 662.357857 - 667.927857
46 671.142857 668.357857 - 673.927857
47 677.142857 674.357857 - 679.927857
48 683.142857 680.357857 - 685.927857
49 689.142857 686.357857 - 691.927857
50 695.142857 692.357857 - 697.927857
51 701.142857 698.357857 - 703.927857
52 707.142857 704.357857 - 709.927857

Regards,
Toshi

  • I recommend the standard fractional loop filter that TI uses on the EVM.  You can find the details in the schematics that is on the TI web: http://www.ti.com/lit/zip/slwc095.

    I recommend a PFD frequency around 32.5 MHz which corresponds to an Rdiv = 2.

    --RJH

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.