LMV225: Suitable for UHF RFID signals in the 900MHz band?

Genius 3505 points

Part Number: LMV225

Hi Support,

Require a detection circuit for the presence of UHF RFID signals in the 900MHz band.
Selected LMV225 as the received RF power detector. Is this a suitable device?

However, ee that the LMV225 is used for RF output power sensing (See its Typical Application in the TI datasheet).
Is there an example that would show RF received power detection?
If not, is there support from TI that could provide an example circuit?

Thanks.

3 Replies