I want to create a 2.8GHz Ultra Low Noise LO, using a 87.5MHz TCXO reference and an external 2.8GHz CRO. Is LMX2541 my best choice for phase noise, rms jitter and cost?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Syed,
The LMX2541 is an excellent choice and has both a low PLL 1/f noise and excellent figure of merit. This is likely to be your lowest jitter solution.
If you want lower cost or current, there are probably other solutions that sarifice jitter. The LMX2531 would normally do this, but the input only goes up to 80 MHz, not 87.5 MHz, so you might need to divide this down for this part. But aside from this, unless you want a lot of outputs, like something from the LMK04800 family, I think that the LMX2541 is the best choice.
Regards,
Dean
Syed,
The difference between these options is the VCO frequency; the PLL is exactly the same.
Because you are bypassing the internal VCO, it makes no difference what version you choose.
Regards,
Dean
Dean: Thank you for the explanation.
I will procure one from Digikey then.
I do have additional questions regarding the loop BW limitations. Would it be possible to communicate via email? My address is sraza@abracon.com
Thanks
Syed