Dear,
we curently test TI board TRF372017 EVM for low bitrate (100kb / OQPSK) application.
BB 1uF decoupling capacitor were replaced by strap. Common mode voltage (1.7V) is generated by a pair of differential amplifier. Input level is 100mVrms single ended.
We notice 2 strange behaviors :
- For I and Q in quadrature/sinus, carrier frequency set to 2400MHz, a parasitic signal appear at Flo-2xFbb and magnitude decrease with increasing BB frequency : (34dBc at Fbb=400kHz / 45dBc at Fbb=1200kHz).
If we decrease BB signal magnitude by 2 (6dB), Flo-Fbb signal is reduce by 6dB and Flo-2xFbb is also reduced by 6dB : doesn't seems to be a distortion.
//// addition on february 13th:
We fine adjust phase between I and Q branch to -1°. Side band was suppressed by 50dB.
No changes were observe on signal Flo-2xFbb
////
- For output carrier frequency set to 2399.999MHz (purple trace), very low level noticed at Flo-2xFbb relative to carrier frequency set to exactly 2400.000MHz (green trace) :
Any idea about this two behaviors?
Last question about datasheet content : what is input BB level and frequency for Carrier Feedthrough and Sideband suppression specifications?
Thanks!
//// addition on february 14th:
We put TRF372017 in LO mode : power up output buffer and TX_DIV then connect spectrum analyzer at LO_OUT signal.
For low frequency on I/Q inputs, around 30kHz, we saw a very clean signal at carrier frequency (2400.000MHz) along with two sidebands at 10dBc ...
These two sidebands were suppressed when power down frequency divider in modulator chain (PWD_TX_DIV). Anyone can tell us how can we overcome this drawback?
Original PLL loop filter have been modified in order to use fractional mode PLL, with a loop bandwidth of 70kHz.
////