Hello,
i want to receiver pocsag format.
so i am disable the address field check and crc check (cc1120 standard packet format).
the data length is used "fixed packet length mode", and gpio-2 to trigger pkt_sync_rxtx event.
then the cc1120 running in sniff mode.
but when the message come in, and the gpio-2 is active.
i am read the rx fifo size and data.
the data always is 0xF9, 0xA2, 0x15, 0xD8, 0xF9, 0xA2, 0x15, 0xD8.....(repeat).
i don't understand why the sync word correct active but the fifo data is wrong.
is it register setting wrong or cc1120 can't receiver?
thanks