Gentlemen,
We are trying to achieve an over-the-air receiver LO synchronization
using a few PLL chips - LMX2531 and LMX2485. We are using SA606 with
450 kHz ceramic filters as AGC amplifier followed by a 74LVC1G04DBV
Schmitt Trigger. Please see the block diagram attached.
When LMX2485 is driven from an external signal source we can get
both PLL#3 and PLL#2 to lock. However, when the incoming RF signal
is present PLL#2 goes off lock and its output becomes a wide-band
noise and PLL#3 never locks again.
I wonder if anybody has done something like this before and can
suggest an appropriate course of action?
A question for the TI professionals (if they read this):
1. does TI have a low cost, small form factor, single chip
reference-less wireless receiver which recovers the LO
frequency directly from the received RF signal?
2. is it possible to get a reference design that accomplishes
such a task?
What is an OSCin jitter spec for LMX2531 and LMX2485?
Please help.