Hi,
Customer is going to use TRF37C75 for mobile communication system.
So, would you please provide Power dissipation(MAX) value?
They strongly requests the data to estimate exactly the power consumption of their system.
Best Regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Customer is going to use TRF37C75 for mobile communication system.
So, would you please provide Power dissipation(MAX) value?
They strongly requests the data to estimate exactly the power consumption of their system.
Best Regards,
Kato
Please disregard my previous post related to Icc dependent on frequency; I was thinking about a different device. The ‘C75 current is very consistent over frequency and over devices. The Histogram of the Icc over devices is shown below. The variation is around +/- 2 mA. –RJH
Icc(mA) #
82 0
83 0
84 1
85 17
86 53
87 33
88 2
89 0
90 0
Kato:
Yes, the data is for devices from one production batch (multiple wafers). At this time I do not have any data from multiple production runs so I cannot comment on lot-to-lot variation; however, given the simplicity of the circuit and the tight tolerance seen on existing data, I do not expect much variability due to process.
--RJH