I have a question about LMH2110 EN pin maximum voltage.
The value in maximum ratings table on p4 of the datasheet and in the pin description is 3.6V
However, in the description section (7.3.3.2 p20), it is written that "the voltage level on the enable must not be higher than 3V to prevent damage"
Which one is correct? 3.0V or 3.6V?
The reason of my question is that I want to interface with a 3.3V signal. Can I have a direct connection or do I need to lower the level to less than 3.0V
Thank you in advance for your help.
Best regards,
pascal