Hi everybody,
I have a TRF7960A EVM and i am trying to read RFID tags that are ISO18000-3 mode 3 compliant. The firmware available on TI Website only supports ISO15693, ISO14443A & ISO14443B tags. However documentation for TRF7960A EVM mentions that the module supports ISO18000 as well. On doing some research, i found that ISO18000-3 mode 3 compliant tags are compatible with same hardware infrastructure that supports ISO15693. To be more specific, the tags i want read are ICODE ILT-M (ISO 18000-3 mode 3/EPC Class-1 HF) from NXP.
Can anyone point me the right direction as to what firmware changes might be required to include support for ISO18000-3 mode 3. Any help would be much appreciated.
Thanks & Regards
Sahil Saini