Hi, I am programming a TRF3750 I think correctly but it is doing some strange things. First the charge pump only ever gets tiny blips <500mV on the output even though it is powered with 7V and has the loop filter circuit of the datasheet on the output CPOut. Is that normal? When I output the R divider it seems to have the correct frequency. I have a 20MHz reference into RefIn and it is divided by 800 to give 25kHz. But when the R divider comes out of muxout, it comes out in bursts, not continuously, is that normal? When I output the N divider out of muxout it is not what I expected. I have a 5MHz input signal and I thought the output of the N divider would be 5MHz / (A+PB) = 25kHz. P is 8, A is 8 and B is 24. But the N divider output is 500kHz. If I input 10MHz with the same divider the N output is 357.1kHz. Which I don't understand.
I have R = 0x110C80, N = 0x001821 and Function = 0x1F8822.
Can anyone help? Thanks.
regards,
Kathryn.