This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF37x73/75 EVM

Other Parts Discussed in Thread: TRF37D73EVM, TRF37D73

Hi,


I would like to buy a TRF37D73 EVM to amplify a signal  with a  frequency of 73 MHz and another signal that ranges from 50 MHz to 800 MHz. It says on the page that the TRF37D73 EVM has a 20dB gain for a 2.5GHz frequency, the TRF37x73 and TRF37x75 EVM User’s Guide doesn't specify the gain for the range from 1MHz to 6GHz where the TRF37D73 is functional. Is there any way to know the gain at a specific point (for instance: 73MHz)?, I would like to know if at this frequency the EVM still has a gain and if it is posible to tune the EVM, is it?.

Regards,

Angel