Hi Sir:
An issue in DTV Band of OFMD modulator from DAC output "DVB-C" mode to TRF3720 REV.C demo kit.
RF detect constellation as MER 29~30dB only in the QAM256. (These Zero-LO mode.)
When I tries IF mode by 6Mhz out band. Then MER up to 38dB in the DVB-C, QAM256 too.
Next lab: I try mode DVB-T mode and verifies again. MER is 38dB in QAM64, DVB-T.
The DAC output is 45MER to IQ input of TRF3720 demo kit(Rev.C).
Also, I had confirm symbol size as band width from 5120, 6120, 6900 ...etc. It's same MER 29~30dB.
And trim balance between LO with IQ offset. Then LO at -65dBm under.
But DVB-T is good quality on demo kit.
Why is not good on Zero-Lo at DVB-C mode??