I have a customer who is seeing the following when testing the LMH2120:
I am using an AN-2064 eval board with a 2.5 Gb/s PRBS input signal as the RF source. I see a strong 6.25 MHz tone on a DC pedestal. The tone amplitude is about 33% of the DC level. Any idea why I might be seeing this tone? I don’t think it’s related to the spectral content of the PRBS signal? I tried lower data rates and get the same tone, so I think the problem is in something I’m doing wrong. I am just sending the output into an o-scope. That part is pretty simple.
I have looked at it with a DVM and that reading is fine. I will however be reading this signal with an ADC and the sampling could become an issue. I have made an LP filter to eliminate the 6.25 MHz tone. It’s still surprising to me that this would show up. I’m not sure if you’re planning to look further into this, but I’m sure than anyone doing high-speed sampling (~ 1MHz) would benefit from its resolution. I did run the fft analysis on the scope and it detected a very pure 6.25 MHz tone and this tone rode on a DC level. The tone did not change amplitude, the the DC level changed as one would expect with a changing RF power level.
Is this something the customer should be seeing? Is this signal coming from the part ar is there something else happening?
Thanks for your help with this!
Richard Elmquist