When spurs appear on the output of this device, there is a magic button called Spur-b-gone that alters some of the parameters to reduce the spurs.
What does this button do, what are the things that change and can this be done is a simple algorithm running on a microcontroller?
Also you seem to adjust a number parameters, including the channel spacing, which presumably want to be fixed at some nominal value and not changed?