Hi
Could you tell me the thermal information of the LMV225SD.
I need theΘja and Θjc.
Best regards,
masa0301
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Actually, they did get this info and already had started working on the model, so I now have results. Please find the info below for LMV225SD, I put in the standard datasheet notes also. Remember, your theta JA is application specific.
Thermal Metrics (1)
Theta JA-High K (2) = 90.9 °C/W
Theta JC, top (3) = 81.3 °C/W
Theta JB (4) = 60.6 °C/W
Psi JT (5) = 4.0 °C/W
Psi JB (6) = 60.8 °C/W
Theta JC, bottom (7) = 11.2 °C/W
(1) For more information about traditional and new thermal metrics, see the Semiconductor and IC Package Thermal Metrics application report (SPRA953).
(2) The junction-to-ambient thermal resistance under natural convection is obtained in a simulation on a JEDEC-standard, High-K board, as specified in JESD51-7, in an environment described in JESD51-2a.
(3) The junction-to-case(top) thermal resistance is obtained by simulating a cold plate test on the package top. No specific JEDEC-standard test exists, but a close description can be found in the ANSI SEMI standard G30-88.
(4) The junction-to-board thermal resistance is obtained by simulating in an environment with a ring cold plate fixture to control the PCB temperature, as described in JESD51-8.
(5) The junction-to-top characterization parameter, ΨJT, estimates the junction temperature of a device in a real system and is extracted
from the simulation data for obtaining RθJA, using a procedure described in JESD51-2a (sections 6 and 7).
(6) The junction-to-board characterization parameter, ΨJB estimates the junction temperature of a device in a real system and is extracted
from the simulation data for obtaining RθJA , using a procedure described in JESD51-2a (sections 6 and 7).
(7) The junction-to-case(bottom) thermal resistance is obtained by simulating a cold plate test on the exposed (power) pad. No specific
JEDEC standard test exists, but a close description can be found in the ANSI SEMI standard G30-88.
73,
Timothy