I want to inject a signal to the ADC input (which is connected to TRF371125 base band output) while the TRF371125 is not enabled (pin 3 = "0"). Is it in tri-state mode (Hi-Z)? Can I inject a 2Vp-p differential sine signal riding on a common mode voltage of 1.5V?
This is for production testing of the ADC and DSP part.
Thanks, Victor Koren.