Hello
My customer wants that the transmitter will be used both for modulated signal and also for high spectral purity CW signal for calibration.
My LO to the modulator is very clean, so I would like to use it, Is there an option to bypass the IQ mixer inside the modulator, or to set value of 0Hz (DC?) at the IQ BB inputs to just pass the LO to output? What would be the conversion loss then? the spectral image?
Thanks