Hi all,
My customer has some questions about TRF370417 specification as belows;
1. What is the absolute maximum ratings of BBIP, BBIN, BBQP and BBQN during normal operation?
2. About the baseband inputs,
according to the datasheet, Vcm is 1.7V as typical value.
When DC connection, is the typical input signal level 98mV-rms?
What is the maximum value?
3. According to the EVM schematics and the EVM Layout, NC pins are connected to GND.
But the datasheet disclibed that All NC pins can be left floating.
Which is the recommended way to make NC floating or connected to GND?
Best regards,
Toshi