I am currently utilizing the TRF3722 in a transmitter design. While testing with the TRF3722EVM eval board (100MHz ref from a microwave source, 25 MHz PFD, and 2800 MHz output), I noticed what seemed like the reference frequency feeding through to the modulated output. See attached picture.
A second test on the eval board showed that with the DAC input disabled, the PFD frequency is also seeming to bleed through. See second attached picture.
The output of the TRF3722 is fed through a low pass filter to reduce the 2nd and 3rd harmonics, but I still have an issue of the reference clock and PFD feedthrough, which can cause "close-in" mixed spur content at the output of an upstream mixer.
Is there a way that I can reduce this feedthrough?
Thank you in advance.
Jon
Reference Feedthrough
DAC/Modulator disabled