TI Home » TI E2E Community » Support Forums » RF & Digital Radio » Design Notes » Design Notes
Share
RF & Digital Radio
  • E2E Wiki
  • /etc... RF /etc... RF
  • Digital Radio (GC Products) Digital Radio (GC Products...
  • High Performance RF Modulators, PLL and VCO products High Performance RF Modulators...
Table of Contents
  • Design Notes

Design Notes

RF & Digital Radio

Welcome to the RF & Digital Radio Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

  • Article
  • History

Design Notes

Rate This

 

To post a question select the type of RF product you are asking about from the table on the top left and then click new post.

 

Comments
  • 32 32 32 32
    May 4, 2010 2:31 AM

    About Zigbee Protocol

  • 32 32 32 32
    May 4, 2010 2:35 AM

    hello everyone.

    who can tell me zigbee mesh network (mesh) routing protocol for that? Is it AODV?

    thanks!!!

  • 2831 2831
    May 8, 2010 11:10 AM

    ABOUT PLL

  • Suno Kim Suno Kim
    May 25, 2010 2:06 PM

    Hello,

    Sombody Help me!

    I have trouble, in application of CC1020.

    When I change stage to Receive mode, then data signal is apeared on the DIO pin, eventhough I short Ant pin to Ground.

    How is it possible?

    I use 3 days to solve this problem, but I still not solve it.

    My Init Sequence is,

      SetupCC1020PD();

     ResetCC1020();

     SetupCC1020All();

     WakeUpCC1020ToTX(0x47);

     CalibrateCC1020(0xA0);

     WakeUpCC1020ToRX(0x47);

     CalibrateCC1020(0xA0);

     SetupCC1020RX(0x47, 0xA0);

    and the Config data is,

     0x0F,  // 0x01, INTERFACE

     0xFF,  // 0x02, RESET

     0x8F,  // 0x03, SEQUENCING

     0x3A,  // 0x04, FREQ_2A

     0x14,  // 0x05, FREQ_1A

     0x99,  // 0x06, FREQ_0A

     0x3A,  // 0x07, CLOCK_A

     0x3A,  // 0x08, FREQ_2B

     0x1F,  // 0x09, FREQ_1B

     0x45,  // 0x0A, FREQ_0B

     0x3A,  // 0x0B, CLOCK_B

     0x44,  // 0x0C, VCO

     0x51,  // 0x0D, MODEM

     0x9B,  // 0x0E, DEVIATION

     0xC6,  // 0x0F, AFC_CONTROL

     0x2F,  // 0x10, FILTER

     0x61,  // 0x11, VGA1

     0x55,  // 0x12, VGA2

     0x2f,  // 0x13, VGA3

     0x2d,  // 0x14, VGA4

     0x20,  // 0x15, LOCK

     0x78,  // 0x16, FRONTEND

     0x47,  // 0x17, ANALOG, RX=47/TX=47

     0x14,  // 0x18, BUFF_SWING

     0x22,  // 0x19, BUFF_CURRENT

     0xAE,  // 0x1A, PLL_BW

     0x34,  // 0x1B, CALIBRATE

     0xF0,  // 0x1C, PA_POWER

     0x00,  // 0x1D, MATCH

     0x00,  // 0x1E, PHASE_COMP

     0x00,  // 0x1F, GAIN_COMP

     0x00   // 0x20, POWERDOWN

    I don't understand Why the Signal is appear on the DIO pin, without input signal.

    Please somebody help me.

    Thanks.

  • T.F. Mulder T.F. Mulder
    May 29, 2010 8:14 PM

    Hi,

    the CC85XXDK contains the parts:

    CC85XXEM

    CC85XX-CC2590EM

    is is possible to get/bye only the CC85XX-CC2590EM (or CC85XXEM) without the complete CC85XXDK

    Theo

  • kamxiao xiao kamxiao xiao
    Aug 2, 2010 4:23 AM

    hello everyone.

    We have a product using the CC2530.The SPI interface of CC2530 connection external FLASH. CC2530 is the SPI master. Use USART1 the alternative1. Hardware connections are as follows. Test found that there is no clock signal output P0.3. When modified to use USART0 of the alternative1, test P0.5, The CC2530 have clock output. Why? If the special requirements of IC, Why did not the notation description in the specification?

  • kamxiao xiao kamxiao xiao
    Aug 2, 2010 4:31 AM

    About cc2530 spi master

  • Sebastien Grenier Sebastien Grenier
    Oct 5, 2010 8:20 PM

    I tried to install the TRF7960 usb drivers unsuccessfully even following  the  SLOU1892C.

    I'm running windows 7 ultimate.

    The software is telling me this error: "invalid entry" even if I try to select the right com port.

    I verified the com port and it's  seem ok.

    I tried to have some answers on E2E community but nothing regarding my problem.

    Could you help me on this issue?

    Regards,

    Sebastien Grenier

  • moncef mabrouk moncef mabrouk
    Dec 8, 2010 1:47 PM

    i need to design a RF remote control swith (to switch ON/OFF network power supply 230v for lighting lamp.

  • ahmed hossam ahmed hossam
    Dec 14, 2010 9:07 PM

    I would like to detail description about the interface between this two RF  kits and DSP kit  

    transmitter   TSW3003EVM-RF Transmit Chain Demonstration Kit

    focus.ti.com/.../tsw3003evm.html

    ====================================

    Receiver  TRF3710EVM Evaluation Module

    focus.ti.com/.../trf3710evm.html

  • Victor Montilla Victor Montilla
    Feb 28, 2011 4:40 PM

    hello,

    My qüestion is about the cc2540 and its development kit. I have a doubt in the schematics design that appears in the document SWRR071. There are 2 inductors between the chip and the antena (ref. 251 and 261), that seem to have a value of 2.0nF in the schematic, but in the components boom they have a value of 2.2nF. Which is the correct value for this components the one that apperas in the schematic, the one that appears in the boom or both?

    Thanks for the answer!

  • Sharath Prasad Sharath Prasad
    Jul 5, 2011 10:59 AM

    CC2591 bias inductor tolerance

  • James A. James A.
    Jul 20, 2011 2:56 PM

    AN068 (swra236a.pdf), Section 5.2.

    I believe the capacitors should be in series with the resistors in the differential to single-ended realization.

    Figure 5, and the whole section assumes the capacitors in shunt configuration.  Is this an error?

  • Aung Myat Lwin52976 Aung Myat Lwin52976
    Dec 7, 2011 3:40 AM

    Hello everyone,

    I purchased CC-6LOWPAN-DK-868 last week. I followed the steps according to CC-6LOWPAN-DK-868 Quick Start Guide and User's Guide. but in step 4(as mention in Quick start Guide) I can't see ipv6 router and only see the error message "No connection to /2001:0:0:0:0:0:11".

    I can see "PHY: 1:00 - Link is Up - 100/Full" using hyperterminal and also found address 2001::22 under "Local Area Connection" when I use Dos command "netsh interface ipv6 show address".

    Here my machine is installed Window 7 Enterprise.

    Anybody, can you help me why my machine can't get ethernet connection with edge router.

  • Robert2787 Robert2787
    Jan 9, 2012 9:53 PM

    I have a SimpliciTI project running well on CCS v4.Now when I migrate the project on CCSv5 I have some errors. It cannot resolve the symbol MAX_APP_PAYLOAD  located in one configuration file. Also when I attempt to change some parameter in the Porject properties Window, the system tells me to look for details of an error in the project.log file.

    I have the following message in this file

    : !ERROR: Build-tools MSP430v3.2.1, or any version compatible with it, is not currently installed! Please migrate the project to one of the supported build-tools first.

    Could someone help me to resolve this problem.

12
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
All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.