Dear ones,
Is there any library by Texas Instrument enabling the FDC2214 communicate with LabView and thus interact with the module via the serial connection , USB , GPIB , or some other ?
LabView commands are used to read and send data through the ports mentioned earlier, called " VISA " , I tried using the VISA for the serial port , but there is an error when you initialize the module , which prevents work with . I do not know if this is because the fdc2214 not support this type of command .
In conclusion, is it possible to communicate with LabVIEW through fdc2214 some library ?, If the answer is " NO" , then, are platform through which I can communicate with the sensor ( C, Java ? ) ?. I hope and has been sufficiently explicit .
I will watch for your answer.
Regards.