Hi all,
Reading the schematic of SNAU178 (page 8) I see three capacitors who's use I don't quite understand.
- CS1 connected between shield 1 and ground 51 pF
- CS2 connected between shield 2 and ground 51 pF
- COFF between CIN-3 and ground 100 pF
I assume the COFF is to demonstrate the offset capabilities of the sensor? Yes?
What are CS1 and CS2 for? I can't find an explanation in the documentation.
Thanks.