I use Fdc2214 in the use of detection ,can not detect the completion of the interrupt signal, How do I set the interrupt to detect the signal?
2: In FDC214 I/O measure a only half of the sine wave, when the capacitance value increases , the amplitude of the sine wave is reduced, and even no sine signal
,if this will affect the accuracy of the measurement, ?