Other Parts Discussed in Thread: FDC2214
Hi,
I am using a custom-designed PCB as a sensor along with the FDC2214EVM. The sensor I am using having one circle at the center and two concentric rings with bigger diameters. Here, I am using the circle at the center and the outermost ring as two plates of a capacitor. According to the datasheet of FDC2214 to measure an unknown capacitance, one terminal of the capacitor has to be connected to one of the channels of the evaluation board and the other terminal of the capacitor has to be connected to the ground. Hence, at present I am connecting the circle at the center of the PCB to CH0 and the outermost ring to the ground point on the EVM pcb.I have shown the connection in the attached figure. The logic I am trying to implement is that as the sensor PCB moves across a surface with considerable change in material permittivity, it will show a change in capacitance at the output. Kindly let me know whether the type of connection is used to implement my idea is correct or not.If this is not the right approach, please suggest me the correct configuration.KindlyFDC2214_Connection.pdf see the attached figure for further clarification.
with warm regards,
Shantanu