I need for a gesture control application 9 capacitive proximity sensors, which are connected on a PCB with a hatch fill on top and bottom, which are driven with an active shield signal from the FDC1004 shield output. Since the FDC1004 has only 4 channels, I intend to use 3 FDC1004 devices with using an I2C multiplexer. I'm now unsure how to wire the hatch fill with the shield output. Each sensor is connected with a shielded coaxial cable to the FDC1004 device.
Is there any recommendation? Can I now connect the hatch fill and the coaxial cable to all three devices on Shield1 port (parallel) or is one connection to one device enough? Or should I wire each coaxial cable of the corresponding device to the shield port and additionally the hatch fill connection to one specific shield pin of device 1,2 or 3 (doesn't matter which one)?
Thanks for the support!