Other Parts Discussed in Thread: FDC1004, , FDC2214
I have an application which needs to monitor oil levels within an EMI-dirty environment. After having a brief play with the FDC1004, it looks like it'll work, but I'm curious about whether I can get any gains from moving to the FDC2### devices? The liquid is non-conductive, and no humans will be anywhere near it: EMI and EMC will be harsh, however.
Obviously my first port of call was the level sensing application note, based on the FDC1004. Was this chip selected as it is better at the level sensing application, or was it selected as being the only part available at the time of writing? If, for example, you were to re-write the technical note now, would the FDC1004 still be device of choice, or assuming FDC2114 was chosen, is there a better sensor layout possible with the differential channels?
Mat