1. I have connected a Capacitive sensor to Ch2 of FDC2114EVM such that both electrodes are connected to the terminals on board. The sensor is designed such that, application of pressure on one face should change the capacitance of the device. I am getting a steady capacitance of apprx. 10 nF initially. Ideally on application of pressure I should get a deviation from this value, but is not the case I observed. The capacitance is varying only when I take my hand near it, just as in case of proximity sensor.
I can observe a clear change in capacitance change with pressure applied using a LCR meter. This EVM would give me the portabiity if it works.
Is it that the slow variation in capacitance due to applied signal, is seen as noise and is being filtered out by the board.
2. Also, are the 18uH and 33pF filter bank built on the board or do I need to put the values on my own.
3. As the EVM feature says it has noise rejection capabiltiy, how do I ensure that the capacitance variation rejected is noise and not the signal.