Other Parts Discussed in Thread: FDC2214
Hi everybody,
I’m working with the FDC2214 and did a first few measurements. In the datasheet of the FDC2214 I saw the very helpful chapter 8.2.4 Recommended Initial Register Configuration Values. But for me it’s not clear, how to calculate the value of CHx_SETTLECOUNT (Page 44, Point 3 (a)). The formula includes the following variable:
Vpk -> I set to 1.68V
fREFx -> I set to 40MHz
C -> means this the capacitive of the sensor (copper plate) or the additional capacitive?
IDRIVEx -> I set to 15 (from Point 2, Page 43)
So my question is, which value I do have to set for C and did I set the other variables correct. I don’t understand how you get the result of 7.5.
Best Regards
Simon Schnider