We're using the FDC1004, and have been happy with the performance of the sensor during our prototyping. Our primary sensors are rectangular, approximately 100mm x 40mm. They follow the surface of a cylinder with a 200mm diameter, so they need to be able to be curved. As we look at methods for manufacturing the sensors in production, I'd be curious if there are any guidelines on the designs of the sensors themselves.
In particular:
-- Does the separation distance between the sensor and the shield have any effect? We've observed that sensors we make using a traditional PCB (with ~1.6mm separation) perform better than ones we made using flexible PCB process (with ~.1mm separation), but that could be an artifact of our prototyping processes. (In this case, worse performance is characterized by more "crosstalk", where we see an increase in channel 2 counts when an object is placed in front of the channel 1 sensor)
-- Should the sensor / shield be solid? Or would a hatched pattern be better in some way?
-- Are there guidelines on the material between the sensor and shield? Obviously we don't want something conductive, but what are good and bad materials?
-- What is the effect of the area of the sensor? Are there upper constraints we should have in mind for the sensor size? For example, if we can cover our sensing area with a zig-zag shape to get a 50% reduction in sensor size, does that impact performance one way or the other?
Thanks!
Rory