Other Parts Discussed in Thread: FDC1004
I have downloaded and installed the TI Provided "Sensing Solution EVM GUI" found on the FDC1004EVM "tools/software" Tab.
I have two FDC1004EVM boards and I can read solid data from both one at a time.
When I plug a single EVM board in it shows up in the window's device manager on COM3. I can read from it. All is good.
When I plug the second board into a 2nd USB port I can see both boards int he device manager. 1 on COM3 and the other on COM4.
I can still read from the COM3 EVM and it responds appropriately. I see no way to ask the GUI to select the COM4 board instead, nor can I seem to launch a second instance of the GUI. Is there any way to use the GUI to interface to multiple EVM boards at once?
If not, does anyone know if an Arduino Library is out there that supports the FDC1004 chip / EVM board?
Thanks